item Warning and Protective Profile D30 R28-90°: For greater safety in production processes

Black and yellow hatching is a striking feature that makes the new Warning and Protective Profile D30 R28-90° from the item Lean Production Building Kit System impossible to miss. The profile offers maximum protection for people, frames and transported goods at exposed areas and in hazardous zones. It is simply clipped onto the flank of a Profile Tube D30 in a matter of just seconds, making it also ideal for temporary use on profiles, as it is easy to install and quick to remove. The elastic chamber of the new Warning and Protective Profile deforms to absorb impacts, thus offering optimum protection for staff and materials alike.

Warning and Protective Profile D30 R28-90° provides all-round protection for all item D30 profiles with the familiar flank geometry. The new profile from the Lean Production Building Kit System encompasses a quarter of the Profile Tube, leaving the rest of the Profile Tube accessible. If required, a D30 profile can also be completely covered on all sides. The striking markings draw attention to hazards in production and other work areas, thus providing an additional safety feature that helps prevent injuries among employees. The new safety component from item is also suitable as impact and scratch protection for all kinds of transported goods and protects frames and individual profiles, too. In the event of an impact, the chamber of the Warning and Protective Profile deforms only momentarily, as the material is elastic. This means any deformation caused by forces is not permanent. The impact protection, with its black and yellow hatching, is also suitable as a temporary means of marking out profiles and structure. As it is simply clipped onto the flank of a Profile Tube D30 and can be removed without leaving a trace, Warning and Protective Profile D30 R28-90° can be fitted after replacing Profile Tubes or making other changes to a frame.

 

Length:          2,075 characters including spaces

As at:             12 November 2018

 

Images:          2

Caption 1:                  Warning and Protective Profile D30 R28-90° offers all-round protection for all item D30 profiles with the familiar flank geometry, while its striking hatched markings make it impossible to miss.          

Caption 2:                  The new safety component is ideal as impact and scratch protection for frames.

 

item Industrietechnik GmbH

item Industrietechnik GmbH is a global market leader in building kit systems for industrial applications and employs around 500 members of staff. It has been designing and marketing construction solutions for machinery, fixtures and plants since 1976. The product portfolio comprises more than 3,500 high-quality components designed for use in machine bases, work benches, automation solutions and lean production applications. Thanks to the inclusion of transport solutions and dynamic elements, the company’s products can cover virtually all working processes, from manual production to automated manufacturing. The highly skilled employees work day in, day out to develop innovative solutions for state-of-the-art mechanical engineering and also offer exceptional consulting services. item is headquartered in Solingen, Germany. Eleven branches and support centres ensure the company is always close to customers in Germany. The group has wholly owned subsidiaries in the USA, China, Mexico, Italy, Poland and Switzerland.

Můžeme Vám osobně poradit?

Žádost o projekt

Pomůžeme Vám při plánování Vašich projektů.
Individuálně a vysoce efektivně.

Konfigurace

Individuální, jednoduché, časově
neomezené on-line plánování.

Online shop

Vždy pohodlné a snadné objednání!
Zadejte svou objednávku!